UG_Wiser Building Management System_WH-00

About the Wiser BMS

The Wiser Building Management System (hereinafter referred to as BMS) is a solution to improve the efficiency and effectiveness of buildings equipped with the Wiser system. Wiser BMS allows setting up schedules for lighting, HVAC, and other systems that ensure they operate efficiently and only when needed. The system offers remote access capabilities, allowing building managers to monitor and control building systems from anywhere. Building managers can track real-time energy consumption, analyze usage patterns, and implement energy-saving measures to reduce costs and improve sustainability.
NOTE: The Wiser BMS UI may vary for each user, depending on their specific requirements.

Benefits

Efficiency: Wiser BMS improves operational efficiency, reducing the time and effort required to manage building operations.

Cost Savings: Enhanced energy management and automation resulting in significant cost savings by reducing energy consumption and maintenance costs.

Comfort and Safety: Wiser BMS ensures that the HVAC, lighting, and security systems operate well, providing a comfortable and safe environment for building occupants.

Temperature Control: You can set the temperature for your different spaces.

Alarms: Different alarms can be triggered based on your specific needs (set up by the Schneider Electric team):

  • Detect abnormal high temperatures caused by unauthorized auxiliary heating methods.

  • Detect a risk of mold proliferation caused by excessive humidity levels.

  • Detect excessive use of domestic hot water.

Applications

Residential Buildings:

  • Social housing complexes.

  • Student accommodations.

  • Retirement homes.

  • Small to extra-large apartment buildings.

Non-residential Buildings:

  • Small schools and daycare centers.

  • Restaurants and cafes.

  • Co-working spaces and small offices.

  • Cultural centers, including community centers, religious sites, small museums, and art galleries.

  • Libraries and standalone retail stores or dealerships.

  • Small entertainment centers, such as cinema theaters, sports clubs, and gaming centers.

The Wiser system is suitable for controlling dwellings or small non-residential buildings that share similar infrastructures with dwellings. For buildings requiring more advanced controls, it is recommended to use an appropriate solution from the Schneider Electric portfolio for commercial and industrial buildings.

The Wiser BMS solution can manage both Wiser setups and installations for non-residential buildings for the same customer. For example, a large shopping mall can include extensive retail areas on the ground floors and dwellings on the upper floors. In this scenario, Wiser BMS is a suitable solution.

Data as a Service

Wiser BMS provides data to building managers to check energy efficiency and operate devices efficiently.

  • Wiser BMS: Enables building managers, facility managers, or maintenance supervisors to operate the devices remotely and monitor energy efficiency.

  • Wiser Home Essential API: Integrates with your existing custom software, allowing you to enhance your system with custom workflows and functionalities.

These services are offered as subscriptions. The Schneider Electric team hosts the data, maintains its accessibility, and the customers use it on demand.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.