Showing 4,771 - 4,780 of 9,846 results

Page 478 of 985
  • Verificar o histórico do dispositivo

    Sensor de fumo 230V Wiser – Guia do utilizador do dispositivo Wiser Home

    Verificar o histórico do dispositivo Verificar o histórico do dispositivo Verificar o histórico do dispositivo Através da aplicação Wiser Home, pode ver a deteção de fumo e de temperatura elevada acedendo ao histórico do sensor de fumo. O histórico do dispositivo é todo armazenado na nuvem. Quando
  • Regulador

    Sistema M y sistema D - Módulo soporte de tecla simple/doble conectado – Guía del usuario del dispositivo Wiser Home

    puede hacer de la misma forma para un regulador de 2 teclas. En la pantalla Inicio, toque . Pulse Dispositivos Luces Regulador para ir a la pantalla Detalles del dispositivo. A Nombre del dispositivo: Pulse para cambiar el nombre del dispositivo. B Localización: Pulse para asignar el regulador a
  • Pairing the device with the Wiser Hub

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the MAC Address and Install Code, then tap
  • About the Wiser BMS

    Wiser BMS – Building Management System – User Guide

    About the Wiser BMS About the Wiser BMS About the Wiser BMS The Wiser Building Management System (hereinafter referred to as BMS) is a solution to improve the efficiency and effectiveness of buildings equipped with the Wiser system. Wiser BMS allows setting up schedules for lighting, HVAC, and
  • Setting the room temperature using the app

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Setting the room temperature using the app Setting the room temperature using the app Setting the room temperature using the app Using the Wiser Home app, you can adjust, set or boost the room temperature. Precondition: Add a Wiser Room Thermostat/ Wiser Temperature/Humidity Sensor in the same room
  • Setting Tariff

    Wiser Home – System User Guide (Spain and Portugal)

    Micromodule Connected Sockets PowerTag Energy Wiser Plug You can set the tariff based on your contract type: Flat rate: The fixed rate for the entire time period of electricity service. Configuring - flat rate. Peak/Off-Peak Hours rate: Peak rate is the rate set to a specific period of time at which
  • Määrittäminen - (huippu/hiljaiset tunnit) hinta

    Wiser Home – Järjestelmän käyttöopas (Ruotsi, Suomi)

    tätä valikossa siirtymistä, jos sinun tarvitsee tehdä muutoksia: Napauta Aloitusnäytöllä Energianhallinta > Tariffi > Sähkö. Napauta (A) ja valitse Käyttöaika (huippu/hiljaiset tunnit). Napauta (B) sopimuksen rajan määrittämiseksi. sopimuksen raja on jo määritetty, kun pääasiallinen PowerTag
  • Identificación del dispositivo

    Unica - Interruptor inalámbrico de una/dos teclas conectado – Guía del usuario del dispositivo Wiser Home

    cortas consecutivas y con gran rapidez del pulsador (A). El interruptor inalámbrico se reactiva durante un minuto y el LED de estado parpadea en verde 5 veces y, a continuación, se para. En la pantalla de Inicio, pulse Dispositivos Interruptor inalámbrico de dos teclas conectado Identificar (A). El LED
  • Controlar o dispositivo com botões de pressão

    Unica - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    interruptor sem fios (< 0,5 s) para ligar/desligar a luz, ou para o definir para um nível de brilho específico (apenas para variadores). Estore Prima ligeiramente o botão de pressão atribuído no interruptor sem fios (< 0,5 s) para abrir/fechar o estore para a percentagem configurada. Momento
  • Ajuste de la localización del dispositivo

    Unica - Toma de corriente inteligente, 1 elemento, 16 A – Guía del usuario del dispositivo Wiser Home

    Ajuste de la localización del dispositivo Ajuste de la localización del dispositivo Ajuste de la localización del dispositivo Puede añadir su dispositivo a cualquier habitación (como el dormitorio, el salón, el comedor, etc.). En la pantalla de Inicio, pulse . Pulse Dispositivos, seleccione en la
Page 478 of 985