Showing 4,791 - 4,800 of 9,846 results

Page 480 of 985
  • Informações técnicas

    Termostato Encastrado Wiser 2 A – Guia do utilizador do dispositivo Wiser Home

    Informações técnicas Informações técnicas Informações técnicas Tensão nominal: AC 230 V ~, 50 Hz Potência nominal: 2 A Consumo de energia Em modo de espera (Psm) : 0,29 W Em modo de espera em rede (Pnsm) : 0,36 W Modo de espera em rede com ecrã (P): 0,5W Tipo de controlo da temperatura: TW
  • LED indications

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the top-right push button 3 times. LED blinks orange, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a few seconds, before
  • LED indications

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times LED blinks orange, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a few seconds, before turning Off
  • Defining Lux setting

    Wiser Motion Sensor – Wiser Home Device user guide

    , tap . Tap Devices Motion Sensor Lux levels (A) to select and define threshold value one of the following option (B): Very dark Dark Bright Very bright Additionally, you can set the sensor lux value by tapping on the Control tab Motion Sensor Device settings Lux levels (A). A lux value represents the
  • Sustitución de las baterías

    Sensor de movimiento Wiser – Guía del usuario del dispositivo Wiser Home

    Sustitución de las baterías Sustitución de las baterías Sustitución de las baterías Para sustituir las baterías: Gire el sensor hacia la izquierda para desbloquearlo de la placa base. Quite los tornillos de la tapa de las baterías para acceder a las mismas. Sustituya las baterías con la polaridad
  • Restablecimiento del dispositivo

    System M y Sistema D - Toma de corriente inteligente, 1 elemento, 16 A – Guía del usuario del dispositivo Wiser Home

    Restablecimiento del dispositivo Restablecimiento del dispositivo Restablecimiento del dispositivo Puede restablecer la toma de corriente a los valores predeterminados de fábrica. Se puede restablecer manualmente en cualquier momento, por ejemplo, si se sustituye el Hub. Presione brevemente el
  • Example of an automation

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    Example of an automation Example of an automation Example of an automation In the example below, you will get a notification in your app when smoke is detected. Go to Automation > to create an automation. To add a condition, tap Add Condition > Device status change > Smoke Alarm. In Select
  • Troubleshooting in Quick Home Connect

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    outlet Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Socket outlet The Wireless switch
  • Configuration d’un programme

    Ovalis - Prise de courant connectée 16A – Guide de l'utilisateur de l’appareil Wiser Home

  • Troubleshooting in Quick Home Connect

    Ovalis - Connected Relay Switch 10 A – Wiser Home Device user guide

    switch Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Relay switch The Wireless switch battery
Page 480 of 985