Showing 51 - 60 of 1,622 results

Page 6 of 163
  • Inbyggd automatisering

    Renova – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enhet

  • Manuelle Einstellung des Timermodus

    System M und System D - Connected Raumtemperaturregler 16 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    Manuelle Einstellung des Timermodus Manuelle Einstellung des Timermodus Manuelle Einstellung des Timermodus Sie können den Boost-Modus manuell aktivieren und deaktivieren.Bei aktivierter Option steigt die Temperatur in den Temperatursteuerungsmodi um 2 °C und über den Sollwert um +2. Zur
  • Integrierte Automatisierung

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    Integrierte Automatisierung Integrierte Automatisierung Integrierte Automatisierung Es gibt drei integrierte Automatisierungsfunktionen, wie z. B. Boost-Funktion, Alle Änderungen zurücksetzen und Abwesend-Betrieb.
  • Away Mode

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    than 16  °C will change. For example, a room set to 5 °C will remain unchanged. Away Mode overrides Boost and schedules, but you can still manually adjust setpoints, boost individual rooms, or turn hot water ON. When active, rooms and hot water display Away Mode values, and hot water will turn OFF
  • Setting the room temperature using the app

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    time ends. When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point. Moving the slider control to the bottom of the bar activates Frost Protection mode. In
  • Setting the room temperature using the app

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    turns it off. When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point. Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.
  • Automatização incorporada

    Termostato Radiador Wiser – Guia do utilizador do dispositivo Wiser Home

  • Away Mode

    Wiser Home – System User Guide (France)

    the away mode. If Boost Mode is active, Away Mode will lower the target temperature of all boosted heaters, if the Boost value is higher than the Away Mode value.
  • Setting the room temperature using the app

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Setting the room temperature using the app Setting the room temperature using the app Setting the room temperature using the app Using the Wiser Home app, you can adjust, set or boost the room temperature. Pre-requisite: Add a Wiser Room Thermostat/ Wiser Temperature/Humidity Sensor in the same
  • Setting the room temperature using the app

    Wiser Underfloor Heating Controller / Connection Strip – Wiser Home Device user guide

    Setting the room temperature using the app Setting the room temperature using the app Setting the room temperature using the app Using the Wiser Home app, you can adjust, set or boost the room temperature. Precondition: Add a Wiser Room Thermostat or Wiser Temperature/Humidity Sensor in the same
Page 6 of 163