DUG_Underfloor Heating Connection Strip_WH-07

Setting the room temperature using the app

Using the Wiser Home app, you can adjust, set or boost the room temperature.

Precondition: Add a Wiser Room Thermostat or Wiser Temperature/Humidity Sensor in the same room where the device is located.

To adjust, set or boost the room temperature:

  1. On the Control tab, tap All devices or a room tab where the device is located.

  2. Use the slider control on the right of the screen to adjust the temperature.

    TIP: You can also adjust the room temperature:
    • By tapping or on the Control tab, in the Heating section of the concerned room to adjust its temperature.

    • When you add it to your Favourites. To know more about Favourite, refer to the Managing Favourites topic in the respective System User Guide.

    NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

    Tap to set the boost time.

    IMPORTANT:
    • Once the boost time is set, the set-point temperature automatically increases by 2 °C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.

    • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

NOTE:
  • The indicates that the room temperature is below the desired temperature (set point), so the heating is on.

  • The indicates that the room temperature is above the desired temperature (set point), so the heating is off.

  • The indicates that the room temperature is higher than the desired temperature (set point), so the cooling is on.

  • The indicates that the room temperature is lower than desired temperature (set point), so the cooling is off.

  • The / indicates that the floor temperature sensor is configured and when the upper/lower limits are reached the room screen will show the floor limit icons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?