DUG_Wiser 16A Relay for Temperature Control_WH-07

Setting the room temperature using the app

Using the Wiser Home app, you can adjust, set or boost the room temperature.

Pre-requisite: Add a Wiser Room Thermostat/Wiser Temperature/Humidity Sensor in the same room where 16A Relay is located.

Adjusting the room temperature

On the Control tab, tap or in the Heating section of the concerned room to adjust its temperature.

TIP: You can also adjust the room temperature:
  • By tapping of the concerned room on the Control tab and using the slider in the device control screen to adjust the room temperature.

    IMPORTANT:
    • Once the boost time is set, the set-point temperature automatically increases by 2° C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.

    • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

  • When you add it to your Favourites. To know more about Favourite, refer to the Managing Favourite topic in the respective System User Guide.

NOTE: If you only have a single device in the Wiser System, the Control tab will not be visible. All functions will be accessible through the Home screen.

Boosting the room temperature

On the device control screen, tap to set the boost time.

TIP: You can boost the room temperature using the Wiser Room Thermostat center button.
IMPORTANT: Once the boost time is set, the set-point temperature automatically increases by 2 °C for the set boost time. After the boost time is over, the set-point temperature returns to the current scheduled event or to the previous set-point temperature.
NOTE: Boost can be stopped at any time by tapping the and selecting it off.

IMPORTANT: If you have installed both PowerTag and Relay, you can monitor the power flow and energy consumption in the Energy tab.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?