DUG_Connected Thermostat 16 A, ZB_WH-05

Setting the room temperature using the app

Using the Wiser Home app, you can adjust the room temperature for heating.

  1. On the Home screen, tap All or room tab.

  2. To select a thermostat, tap .

  3. Use the slider control and set the room temperature for heating.

    NOTE:
    • The indicates that the room temperature is below the desired temperature (set point), so the heating is on.

    • The indicates that the room temperature is above the desired temperature (set point), so the heating is off.

    TIP: Tapping you can set the boost time and turns it off.
    IMPORTANT:
    • When the boost time is set, the system automatically increases the set-point temperature by 2 °C for the duration of the boost. Once the boost period ends, the temperature returns to the last set-point.

    • Moving the slider control to the bottom of the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.