Showing 5,111 - 5,120 of 9,846 results

Page 512 of 985
  • Installing the device

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    Installing the device Installing the device Installing the device Refer to the installation instruction supplied with this product. Instruction manual links: Connected Thermostat Insert 2 A (S520619, S530619, S540619) Connected Thermostat Insert 2 A (S920502, S940502) Selecting the installation
  • Configuring - feed in tariff

    Wiser Home – System User Guide (Spain and Portugal)

    Insights page, tap Find out more and read the Feed-in Tariff onboarding information. Tap to close the overlay screen. If you have not configured your Feed-in tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks. If you have closed the reminder splash screen, you can
  • Installing the device

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Installing the device Installing the device Installing the device Refer to the Connected Thermostat Insert 16 A installation instruction supplied with this product. Refer to the Connected Thermostat Module, ZB installation instruction supplied with this product. Selecting the installation site:In
  • Control del sensor de movimiento

    Sensor de movimiento de exterior ARGUS 360 – Guía del usuario del dispositivo Wiser Home

    habitación en la que se encuentra el sensor de movimiento. Si solo tiene un dispositivo en el sistema de Wiser, la pestaña Control no será visible. Se podrá acceder a todas las funciones a través de la pantalla Inicio. Seleccione en la lista (A) el sensor de movimiento requerido. Seleccione el tiempo durante el cual debe funcionar el dispositivo conectado. Si es necesario, toque el icono del dispositivo para activarlo o desactivarlo.
  • Configuring - feed in tariff

    Wiser Home – System User Guide (France)

    Insights page, tap Find out more and read the Feed-in Tariff onboarding information. Tap to close the overlay screen. If you have not configured your Feed-in tariff, a push notification will be sent after 2 weeks and the last reminder after 6 weeks. If you have closed the reminder splash screen, you can
  • Abwesenheitsmodus

    System M und System D - Connected Raumtemperaturregler 16 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    Abwesenheitsmodus Abwesenheitsmodus Abwesenheitsmodus Wenn der Abwesenheitsmodus (A) aktiviert ist, werden alle Räume auf die Abwesenheits-Temperatur eingestellt (standardmäßig 16 °C). Wenn diese Option aktiviert ist, wird ein Häkchen in der Seite „Automatisierung“ angezeigt. Sie finden sie im Menü
  • Using the device

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Using the device Using the device Using the device The control panel of the thermostat(s) allows you to view and adjust the temperature and access various settings. Thermostat control panelOn the group thermostat control panel page, you can see the following: A Turning the toggle switch ON
  • Using the device

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Using the device Using the device Using the device The control panel of the thermostat(s) allows you to view and adjust the temperature and access various settings. Thermostat control panelOn the group thermostat control panel page, you can see the following: A Turning the toggle switch ON
  • Impulsionar tudo

    Termostato Radiador Wiser – Guia do utilizador do dispositivo Wiser Home

    Impulsionar tudo Impulsionar tudo Impulsionar tudo Pode aplicar um impulso de +2 °C durante 1 hora em cada divisão do sistema. Não afetará, de todo, a água quente. Como se trata de uma "ação pontual", pode encontrar Impulsionar tudo (A) no menu "Automatização", clicando no separador "Automatização" na parte inferior do ecrã Inicial.
  • Laitteen tunnistaminen

    Wiser-ovi-/ikkunatunnistin – Wiser Home -laitteen käyttöopas

    Laitteen tunnistaminen Laitteen tunnistaminen Laitteen tunnistaminen Wiser Home -sovelluksella voit tunnistaa anturin muista huoneessa olevista laitteista. Valitse aloitusnäytössä . Herätä tunnistin (paina toimintopainiketta). Valitse Laitteet Ovi-/ikkuna-anturi Tunnista (A). Lisäksi voit tunnistaa
Page 512 of 985