Installing the device
Instruction manual links:
-
Connected Thermostat Insert 2 A (S520619, S530619, S540619)
-
Connected Thermostat Insert 2 A (S920502, S940502)
Selecting
the installation site:
In order for the thermostat to be operated, the internal temperature
sensor must be protected as far as possible against external influences
and temperature fluctuations. This helps to guarantee reliable detection
of the room temperature.
The following should therefore
be taken into account when considering the installation site:
-
Minimum installation height: 1.5 m above the floor.
-
Do not install too close to windows, doors or ventilation openings.
-
Do not install above heaters or other heat sources.
-
Do not cover or install behind curtains.
-
Avoid direct sunlight and light from lamps.
-
Do not install in power strips above or next to components that produce heat, such as dimmers or electronic switches.
-
Mounting on the cavity wall requires proper sealing of the conduit box or installation tube, to prevent airflow from affecting temperature sensor performance.