DUG_Exxact - ZB Thermostat 16 A_WH-01

Using the device

The control panel of the thermostat(s) allows you to view and adjust the temperature and access various settings.

Thermostat control panel

On the group thermostat control panel page, you can see the following:
A

Turning the toggle switch ON activates the selected schedule.

B

Allows you to edit an existing schedule.

C

Allows you to add the device to the Favourites section in the Home screen. When you add it to your Favourites. To know more about Favourites, refer to the Managing Favourites topic in the respective System User Guide.

D

Allows you to update the room details (name, location etc.).

E

The sliding bar to adjust the temperature.

F

The set-point temperature value.

G

Tap the (boost icon) (G) to set a time duration for which the setpoint temperature will increase by 2 °C.
When you tap the (boost icon) (G), you can choose one of the following time durations:

  • 30 min

  • 1 hr

  • 2 hr

  • 3 hr

  • Off

H

The current temperature value.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?