Showing 521 - 530 of 1,100 results

Page 53 of 110
  • Insikter

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    Home Smart, Schneider Charge, EV-uttag) eller resistiva vattenpannor (som styrs med en strömställarpuck). Den förlitar sig på att användarna svarar på rutinfrågor. Se Wiser Home AI för detaljerad information. Du kan ändra den visade tidsramen (dagar, månader och år). Om du har installerat PowerTag på solenergi eller solenergi med batteri är Mina besparingar tillgängligt för att visa spar- och intjäningshistorik.
  • Aikataulun määrittäminen

    Exxact - kaksoispistorasia 16A – Wiser Home -laitteen käyttöopas

    -valikkoon. Valitse Smart-pistorasia kohteesta KOSKEE valikko ja napauta Luo. Seuraavassa näytössä näkyy oletuksena viikon tapahtuma, jota voi muokata. Napauta jos haluat lisätä tapahtuman, kuten TILA (päällä/pois) ja AJANKOHTA (auringonnousu/auringonlasku tai tietty aikaväli). Tallenna aikataulu
  • À propos du document

    EVlink Home Smart – Guide d'utilisation de l'appareil Wiser Home

    À propos du document À propos du document À propos du document Objectif du document Ce document fournit des conseils sur l'installation, la mise en service et l'utilisation du chargeur de véhicule électrique EVlink Home Smart avec l'application Wiser Home. Il explique comment configurer les
  • Sistema de Antidisparo EVlink Home

    EVlink Home Smart – Manual do utilizador do dispositivo doméstico Wiser

    utilizado com a Smart EVlink Home. Não utilize com outros dispositivos elétricos. Instalar o sistema de antidisparo Consulte as instruções de instalação fornecidas com este produto. Sistema de antidisparo EVlink Home 1P+N, EVA1HPC1 Sistema de antidisparo EVlink Home 3P+N, EVA1HPC3 Vídeo de instalação: Instalação do sistema de antidisparo
  • Google Home

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    Google Home Google Home Google Home Google Home is a brand of smart speakers that works like Alexa. You can use Google Assistant to request information or perform an action using a variety of commands.” Common Wiser commands for Google Home: Inquiry: “OK, Google, is the hot water on?” Hot Water
  • Example of an automation

    Wiser Plug – Wiser Home Device User Guide

    information and tap OK. To set the time, tap When > Add time > Period of time > Day time > Set. To add an action, tap Then > Add an action > Control a device > Smart Plug > Set. You can turn on/off the plug. Read the information and tap OK. Enter the name of the automation
  • About the device

    Wiser Radiator Thermostat – Wiser Home Device user guide

    individual room control with ultimate comfort, convenience, and practicality. Features of the Thermostat: Mobile control anytime, anywhere with the Wiser app Works with Amazon Alexa & the Google Assistant Full transparency with Insights and the Heat Report Smart modes for maximum energy efficiency
  • About the device

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Insights

    Wiser Home – System User Guide (Germany, Austria)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Google Home™

    Airzone Plenum and Aidoo Pro - Air conditioner – Wiser Home Device user guide

    Google Home™ Google Home™ Google Home™ Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.” Common Wiser commands for Google Home™: Inquiry: “OK, Google, is the
Page 53 of 110