DUG_Ovalis - Wireless Switch_WH-04

About the device

The Connected Wireless Switch 1-gang/2-gang (hereinafter referred to as Wireless switch) is a battery-powered Wireless switch that is used to control a group of Zigbee devices (such as light/shutter) within the same Zigbee network.

The Wireless switch can be configured through the Wiser Home app.

Advantage of using a Wireless switch:

  • Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones.

  • Easy to mount on the wall: no wiring required.

Features of a Wireless switch:

  • Add various actions (such as lighting/shutter control) to the Wireless switch.

  • Add moments to the Wireless switch (such as Movie Night Moment/Good Night Moment).

  • Low battery notification.

    NOTE: This device user guide shows pairing, configuring and other features of Wireless switch 2-gang. The same applies for Wireless switch 1-gang.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?