Showing 5,431 - 5,440 of 9,846 results

Page 544 of 985
  • Definir alarmes

    Micromódulo de potência Wiser – Guia do utilizador do dispositivo

    Definir alarmes Definir alarmes Definir alarmes Através da aplicação Wiser Home, pode definir alarmes para notificar o consumo excessivo ou a ausência de consumo de cargas. Cada dispositivo pode ter um alarme de consumo excessivo e um de ausência de consumo.Para configurar alarmes: No ecrã Inicial
  • Getting to Know the Wiser System

    Wiser Home – System User Guide (Spain and Portugal)

    reports for connected Wiser devices. With a personal account and the Wiser Home App on a smartphone you can control and monitor connected Wiser devices from anywhere where the internet is available for both mobile phone and the Hub.
  • Bloqueo de la interfaz de usuario

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    los niños pequeños cambien las temperaturas de su habitación jugando con los termostatos. En la pantalla Inicio, toque . Toque Dispositivos Bloqueo parental (A) para bloquear o desbloquear el control del termostato. Cuando el bloqueo del termostato está activo, un aparecerá junto al termostato.
  • Tarifa

    Schneider Charge – Guía del usuario del dispositivo Wiser Home

    cálculos de costes, es importante proporcionar los datos de tarifa correctos. Esto permite que el sistema refleje el coste real de su consumo de energía, lo que le ayuda a comprender mejor su consumo y a gestionar sus gastos de forma eficaz.El coste del consumo de energía se basa en el tipo de
  • Handling QR code Issues

    Wiser Home – System User Guide (Sweden, Finland)

    Handling QR code Issues Handling QR code Issues Handling QR code Issues Condition Action If you are unable to find the QR code. Tap I can't find the correct QR code and proceed to Adding a Device. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR
  • Energy Domain with Grid

    Wiser Home – System User Guide (Sweden, Finland)

    Energy Domain with Grid Energy Domain with Grid Energy Domain with Grid If you have an energy device installed, like a PowerTag E, the Energy Centre will be available. In the Energy Centre, you can monitor your energy consumption and production, view detailed history, and get information on energy
  • Setting the device location

    Exxact - Connected Relay Switch 10 A – Wiser Home Device user guide

    open setup screen. On the Device Setup screen, you can enter New room name (A) or select an existing room from the list (B). If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C). Once changes are done, tap Submit (D).
  • Slå på/av enheten med appen

    Exxact – Strömställare 10 A uppkopplad – Bruksanvisning för Wiser Home-enhet

    Slå på/av enheten med appen Slå på/av enheten med appen Slå på/av enheten med appen På fliken Kontroll trycker du på Alla enheter eller den rumsflik där enheten finns. Tryck på (A) för att slå på/stänga av strömställaren. Du kan också slå på/stänga av enheten från skärmen Hem när du lägger till den
  • Laitteen käyttäminen

    Exxact - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

    Laitteen käyttäminen Laitteen käyttäminen Laitteen käyttäminen Termostaatin (termostaattien) ohjauspaneelissa voit tarkastella ja säätää lämpötilaa sekä käyttää eri asetuksia. Termostaatin ohjauspaneeliRyhmätermostaatin ohjauspaneelisivulla on seuraavat tiedot: A Kun kytkin käännetään asentoon ON
  • Editing an automation

    Odace - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    the settings. To remove a condition, slide the condition towards left and then tap (A) to delete it. Tap ⊕ Add conditions (B) to add new condition. To change the order of actions, tap the Then option, and hold an action, then drag and drop to the desired position. Tap Save to save the changes.
Page 544 of 985