Showing 571 - 580 of 1,100 results

Page 58 of 110
  • Om enheden

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

    Om enheden Om enheden Om enheden Wiser Smart Plug (herefter kaldet stik) bruges som stikadapter til at styre forskellige elektriske enheder som f.eks. gulvlamper, radioer eller kaffemaskiner manuelt eller ved hjælp af Wiser-appen. Stikket kan også overvåge strømforbruget for tilsluttede enheder
  • Acerca del documento

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Acerca del documento Acerca del documento Acerca del documento Objeto Este documento proporciona orientación sobre la instalación, puesta en marcha y uso del cargador de vehículos eléctricos EVlink Home Smart con la app Wiser Home. Explica cómo configurar los ajustes de red, gestionar los modos de
  • Felsökning

    Schneider Charge – Användarhandbok för Wiser Home-enhet

    procedur som beskrivs i avsnittet "Drift". Kontakten är ansluten till ett elfordon men laddas inte, LED-lampan blinkar blått. Kontrollera att du inte har ett pågående schema via programmet för smart laddning som förhindrar laddning av bilen. Om du har installerat anti-tripping-modulen kan den
  • Google Home™

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Google Home™ Google Home™ Google Home™ Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.” Common Wiser commands for Google Home™: Inquiry: “OK, Google, is the
  • About the device

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Modo de carga

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Modo de carga Modo de carga Modo de carga Con la aplicación Wiser Home, puede administrar el modo de carga. En la pestaña Control, pulse Todos los dispositivos > EVlink Home Smart. En la página del panel de control del dispositivo, toque Modo de carga. En el menú EV Charging Mode, seleccione una
  • Insights

    Wiser Home – System User Guide (Denmark)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Setting up a schedule

    Unica - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Setting up a schedule

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Setting up a schedule

    LK FUGA® - Wiser wireless socket outlet 1½ M – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
Page 58 of 110