Showing 581 - 590 of 1,457 results

Page 59 of 146
  • Criar uma automatização

    Unica - LED Variador de Luz Conectável – Manual do utilizador do dispositivo doméstico Wiser

    ausente também pode acionar uma automatização para ligar as luzes, fechar o estore, etc. Consulte o tópico Modo Away no respetivo Manual do Utilizador do Sistema. Podem ser adicionadas no máximo 10 condições. Neste exemplo, iremos selecionar Alteração do estado do dispositivo e escolher um dispositivo
  • Exemple d’automatisme

    Wiser Prise Intelligente – Guide de l'utilisateur de l’appareil Wiser Home

    Exemple d’automatisme Exemple d’automatisme Exemple d’automatisme Dans l’exemple ci-dessous, si le mode Absence est activé en Journée, la prise s’éteint. Accédez à Automatismes > pour créer un automatisme. Pour ajouter une condition, appuyez sur Ajouter condition > Mode Absence > Mode
  • Troubleshooting

    Ovalis - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Troubleshooting

    Odace - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Troubleshooting

    Exxact - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    overheating. Reduce load. Change load. Check wiring between the push button and the dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Dépannage

    Wiser micromodule pour interrupteur – Guide de l'utilisateur du dispositif Wiser Home

    possible Solution L’appareil ne peut pas se connecter à la passerelle. Après 3 pressions, le voyant de l'appareil clignote en vert/rouge pendant 30 s. Cela ne s'applique pas aux modèles Zigbee ® plus récents. Le mode d’appairage a changé. Réinitialisez l'appareil. Après la réinitialisation, appuyez 4
  • Troubleshooting

    Odace - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    overheating. Reduce load. Change load. Check wiring between the push button and the dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Appairage du dispositif avec la passerelle Wiser

    Odace - Interrupteur simple/double sans fil connecté – Guide de l'utilisateur du dispositif Wiser Home

    d’appairage réussi s'affiche uniquement si vous êtes connecté en tant que Propriétaire du logement. L’interrupteur sans fil est maintenant répertorié dans l’onglet Contrôle sous les onglets Tout et Pièce. Astuce : Si l’interrupteur sans fil est configuré en mode 2 Boutons et que vous souhaitez le
  • Affichage LED

    Unica - Interrupteur de commande de volet connecté – Guide de l'utilisateur de l’appareil Wiser Home

    Affichage LED Affichage LED Affichage LED Appairage Action de l’utilisateur Affichage de la LED État Appuyez 3 fois sur le bouton-poussoir La LED clignote en orange une fois par seconde. Le mode d’appairage est actif pendant 30 secondes. Une fois l’appairage terminé, la LED s’allume en vert pendant
  • Setting the lux level

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    . To adjust the lux level: On the Device Details screen, tap Lux level. Select one of the following modes: Day Mode: For the devices which should be active during the days and the nights. The device operates irrespective of any lux value. Night Mode: For the devices which should be active in low light
Page 59 of 146