Showing 581 - 590 of 1,622 results

Page 59 of 163
  • Exemple d’automatisme

    Wiser Prise Intelligente – Guide de l'utilisateur de l’appareil Wiser Home

    Exemple d’automatisme Exemple d’automatisme Exemple d’automatisme Dans l’exemple ci-dessous, si le mode Absence est activé en Journée, la prise s’éteint. Accédez à Automatismes > pour créer un automatisme. Pour ajouter une condition, appuyez sur Ajouter condition > Mode Absence > Mode
  • Troubleshooting

    Ovalis - Connected Universal Push-button Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Troubleshooting

    Odace - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    . Reduce load. Change load. Check wiring between the push button and the Dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Troubleshooting

    Exxact - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    overheating. Reduce load. Change load. Check wiring between the push button and the dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Example of an automation

    Wiser Plug – Wiser Home Device User Guide

    Example of an automation Example of an automation Example of an automation In the example below, if away mode is enabled during Daytime, then Plug will turn off. Go to Automation > to create an automation. To add a condition, tap Add Condition > Away Mode > Enabled away mode (A). Read the
  • Dépannage

    Wiser micromodule pour interrupteur – Guide de l'utilisateur du dispositif Wiser Home

    possible Solution L’appareil ne peut pas se connecter à la passerelle. Après 3 pressions, le voyant de l'appareil clignote en vert/rouge pendant 30 s. Cela ne s'applique pas aux modèles Zigbee ® plus récents. Le mode d’appairage a changé. Réinitialisez l'appareil. Après la réinitialisation, appuyez 4
  • Troubleshooting

    Odace - Connected Multiwire Universal Rotary Dimmer LED – Wiser Home Device user guide

    overheating. Reduce load. Change load. Check wiring between the push button and the dimmer. Flickering at minimum brightness. Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device). Change the load (if the minimum brightness is insufficient). Set to RL LED mode
  • Dépannage

    Unica - Interrupteur variateur universel LED connecté – Guide de l'utilisateur de l'appareil Wiser Home

    31LCDA). Modifiez la charge (si la luminosité minimale est insuffisante). Réglez sur le mode RL-LED. Scintillement Modifiez la charge. Réglez sur le mode RL-LED. Capacité de variation légère uniquement Modifiez la plage de variation. Réglez sur le mode RL-LED. Modifiez la charge (si la charge est
  • Dépannage

    Odace - Poussoir variateur connecté universel LED 2 fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    ). Modifiez la charge (si la luminosité minimale est insuffisante). Réglé sur Mode RL LED. Scintillement Modifiez la charge. Réglé sur Mode RL LED. Capacité de variation légère uniquement Modifiez la plage de variation. Modifiez la charge (si elle est incompatible avec le variateur). Réglé sur Mode RL LED
  • Dépannage

    Odace - Variateur rotatif connecté universel LED 2fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    ). Modifiez la charge (si la luminosité minimale est insuffisante). Réglé sur Mode RL LED. Scintillement Modifiez la charge. Réglé sur Mode RL LED. Capacité de variation légère uniquement Modifiez la plage de variation. Modifiez la charge (si elle est incompatible avec le variateur). Réglé sur Mode RL LED
Page 59 of 163