Showing 5,861 - 5,870 of 9,846 results

Page 587 of 985
  • Tips and Advice

    Wiser Home – System User Guide (Denmark)

    available tips. Each tip has two options: You can perform this action only if you are connected to internet. Show Me: Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options: Mark as Done If you find the
  • Tekniska data

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    = Reglernoggrannhet Maximal ström Resistiv belastning: max. 16 A, 3520 W Induktiv belastning: max. 4 A Plintar: Skruvplintar för max. 2,5 mm², 0,5 Nm Neutralledare: Krävs Omgivningstemperatur: 0 till 40 °C Relativ luftfuktighet: Max. 90 %, icke-kondenserande Temperaturnoggrannhet: max. ±0,5 °C (inom intervallet 4
  • Technical Data

    Wiser 16 A Relay for Temperature Control – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Rated voltage: 230 V, 50 Hz (AC ONLY) Power consumption: 7.3 W Purpose of control: Electrical Control, Manual + Automatic Control, Sensing Control Type of load and rated current: 16 A Resistive or (3A) Inductive Load Circuit for pilot load (FP) Not
  • Troubleshooting in Quick Home Connect

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Micro module light switch Micro module shades control Multiwire micro module dimmer Rotary dimmer Push–button dimmer Socket outlet Relay switch Blind control switches The Wireless switch
  • Solución de problemas

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    . Acerque el Wiser Hub al termostato. Utilice el enchufe inalámbrico Wiser para aumentar el rango. No se puede conectar al Wiser Hub (LED rojo intermitente) Mala señal entre el Wiser Hub y el termostato. Los dispositivos no tienen alimentación (termostato/Wiser Hub/red Wi-Fi ®). Vuelva a conectar el
  • Tips and Advice

    Wiser Home – System User Guide (Sweden, Finland)

    available tips. Each tip has two options: You can perform this action only if you are connected to internet. Show Me: Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options: Mark as Done If you find the
  • Tips and Advice

    Wiser Home – System User Guide (UK, Ireland)

    available tips. Each tip has two options: You can perform this action only if you are connected to internet. Show Me: Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options: Mark as Done If you find the
  • Tekniska data

    Renova – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enheter

    = Reglernoggrannhet Maximal ström Resistiv belastning: max. 16 A, 3520 W Induktiv belastning: max. 4 A Plintar: Skruvplintar för max. 2,5 mm², 0,5 Nm Neutralledare: Krävs Omgivningstemperatur: 0 till 40 °C Relativ luftfuktighet: Max. 90 %, icke-kondenserande Temperaturnoggrannhet: max. ±0,5 °C (inom intervallet 4
  • Indicaciones LED

    Sistema M y sistema D - Módulo soporte de tecla simple/doble conectado – Guía del usuario del dispositivo Wiser Home

    se ilumina en verde durante un tiempo antes de apagarse. Restablecimiento del dispositivo Acción del usuario Indicación LED Estado Accione el pulsador 3 veces y manténgalo pulsado una vez durante >10 s. Después de 10 s, el LED empieza a parpadear en rojo. El dispositivo se encuentra en modo de restablecimiento. Los ajustes de fábrica se restablecen tras 10 segundos. A continuación, se reinicia el dispositivo y el LED se ilumina en naranja.
  • Ajuste manual de la temperatura de la sala

    Termostato de radiador Wiser – Guía del usuario del dispositivo Wiser Home

    temperatura. El LED rojo se iluminará durante 5 segundos. En la dirección « -» para reducir la temperatura. El LED azul se iluminará durante 5 segundos. Cuando se gira la tapa del termostato, la temperatura de consigna aumenta/disminuye en 2 °C con respecto a la temperatura actual de la habitación
Page 587 of 985