DUG_Micro Module Light Switch_WH-07

Turning the puck On/Off using app

  1. On the Control tab, tap All devices or the room tab where the device is located.
  2. Tap (A) to turn on/off the puck.
    TIP: You can also turn the device on/off from the Home screen when you add it to your Favourite.
    To know more about Favourite, refer to the Manage Favourite topic in the respective System User Guide.
    NOTE: The Control tab will not be visible if you have only a single device in the Wiser System. All functions will be accessible through the Home screen.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.