Showing 5,891 - 5,900 of 9,846 results

Page 590 of 985
  • Technical Data

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    Connecting Terminals Screwless terminals 2x 1.5 mm² (N) 1x 1.5 mm² (L) 1x 1.5 mm² (Load) Ambient temperature 5 … 25 °C (temporarily up to 35 °C) External fuse protection max. 16 A circuit breaker Nominal current 2x 5 A, cosφ = 0.6 Operating frequency 2405 ... 2480 MHz Max. radio-frequency power transmitted < 10 mW Communication protocol Zigbee 3.0 certified
  • Troubleshooting in Quick Home Connect

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    -button module Wireless switch not able to control the device reliably. The Wireless switch and the device are too far away from each other. Place the Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Push-button module The Wireless
  • Caractéristiques techniques

    Wiser Centrale de Câblage pour Planche – Guide de l'utilisateur de l’appareil Wiser Home

    alimentation : Relais normalement ouverts Sans fil : 2,4 GHz (bidirectionnel, maillage) Plage de signal : 30 m d’espace libre Puissance de signal maximale : 14 dBm (25 mW) Classe de pollution : 2 Classe d’énergie : IV = 2 % Classe de logiciel : A Calibre du fusible : 3,15 A Relais : Normalement ouverts 2(1
  • Tips and Advice

    Wiser Home – System User Guide (France)

    available tips. Each tip has two options: You can perform this action only if you are connected to internet. Show Me: Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options: Mark as Done If you find the
  • Avancerade inställningar

    PowerTag Energy – Wiser Home Bruksanvisning för enheten

    inställningar. Tryck på OK när du uppmanas att bekräfta i fönstret med en varning. Följ något av dessa steg baserat på kravet: Om du har installerat ett nytt elnätsanslutet solenergisystem. Se Parkoppla enheten med ett elnätsanslutet solenergisystem. Om du har tagit bort solenergisystemet trycker du på (A
  • Personalized Energy Insights (Estimated energy)

    PowerTag Energy – Wiser Home Device user guide

    Personalized Energy Insights (Estimated energy) Personalized Energy Insights (Estimated energy) Personalized Energy Insights (Estimated energy) To view the History and Insights of estimated energy consumption with similar homes: History On the bottom navigation bar, tap > History. Tap (A) and
  • Technical data

    PowerTag Energy – Wiser Home Device user guide

    % Phase-to-phase 380...415 V AC ± 20 % Un 3P+N Phase-to-neutral 220...240 V AC ± 20 % Phase-to-neutral 380...415 V AC ± 20 % Phase-to-neutral 120...137 V AC ± 20 % Phase-to-neutral 208...240 V AC ± 20 % Frequency 50/60 Hz Maximum current Imax 63 A Basic current Ib 10A Saturation current 130 A Maximum
  • Tips and Advice

    Wiser Home – System User Guide (Spain and Portugal)

    available tips. Each tip has two options: You can perform this action only if you are connected to internet. Show Me: Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options: Mark as Done If you find the
  • About Signal Strength

    Wiser Home – System User Guide (UK, Ireland)

    About Signal Strength About Signal Strength About Signal Strength Zigbee signal strength or RSSI (Received Signal Strength Indicator) indicates the signal quality between your devices and the Wiser hub. The Closer the RSSI value is to 0, the better the signal. For example, an RSSI of -50dBm is a
  • Troubleshooting in Quick Home Connect

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Wireless switch in a position closer to the device. The Wireless switch lost pairing. Pair the device again. Refer to Micro module light switch Micro module shades control Multiwire micro module dimmer Rotary dimmer Push–button dimmer Socket outlet Relay switch Blind control switches The Wireless switch
Page 590 of 985