System User Guide Wiser Home (France) - 14

Tips and Advice

Provides personalized tips based on the devices you own, helping you optimize their use and improve energy efficiency.

On the Home screen > Tips and advice, scroll horizontally to view three most important tips or tap See all to view complete list of available tips.

Each tip has two options:
NOTE: You can perform this action only if you are connected to internet.
  • Show Me:  Tap a tip or tap Show Me to view the complete tip along with any actions you may need to take. After reviewing the tip, you can choose further options:

    Mark as Done

    If you find the tip relevant and have performed the necessary actions, tap this option to move it to the Archived > Done folder, indicating that you have completed or implemented it.

    Not for Me

    After reading the complete tip, if you still think it is irrelevant to you, tap this option to move it to Archived > Discarded folder.

  • Not for Me: Tap on this option to move the tip directly to the Archived folder if it doesn't apply to you.

Archived Tips

All tips marked as Not For Me or Mark as Done are stored in the Archived folder.

  • The tips which are chosen as Not For Me will be moved to Archived > Discarded folder.

  • The tips which are chosen as Mark as Done will be moved to Archived > Done folder.

To view/retrieve a tip:

  1. On the Home screen, under Tips and Advice, tap See All.

  2. Tap (A) to go to the Archived folder.

  3. Select the desired tip and tap Show me.

  4. Tap Bring it Back to restore it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.