Showing 631 - 640 of 1,100 results

Page 64 of 110
  • Skapa ett scenario

    Wiser Smart kontakt 16 A – Användarhandbok för Wiser Home-enhet

  • Raumdetails

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    Signalstärke. Diese Funktion ist für Wiser Smart Plug Geräte nicht verfügbar. C Tippen, um den Raum zu löschen. Das Entfernen eines Raums sollte nach der Einrichtung Ihres Zuhauses nicht erforderlich sein; dies ist jedoch jederzeit möglich. Wenn Sie einen Raum löschen, werden alle diesem Raum
  • Configuring - flat rate

    Wiser Home – System User Guide (Belgium)

    applicable only if you have installed Water Heater/EV Socket/Schneider Charge/EVlink Home Smart in your home. Tap after setting the contract limit. Tap (C) and select a subscription type (D) (refers to recurrent fee). Enter a value in the Cost (€) (E) field and tap Set. The Fixed Charges is applied to
  • Konfiguration - fast takst

    Wiser Home – Systembrugervejledning (Danmark)

    den er indstillet forkert, fungerer den måske ikke som forventet og kan resultere i, at strømmen går. Tryk på Fortsæt, hvis du vil fortsætte. Anti-Tripping er kun tilgængelig, hvis du har installeret Vandvarmer/EV-udtag/Schneider Charge/EVlink Home Smart i dit hjem. Tryk på , når du har indstillet
  • About the device

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Zigbee network. The device can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to install on the wall: no
  • Eco Mode

    Wiser Home – System User Guide (France)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Personliga energiinsikter (uppskattad energi)

    PowerTag Energy – Wiser Home Bruksanvisning för enheten

    över hela området. Om EVlink Home Smart till exempel inte används mycket i oktober visas det i kortet Andra (D). Det uppdaterade förbrukningsvärdet visas i uppdelningsdelen när du rullar ned. De anpassade etiketterna för laster är grupperade i uppdelningen Andra (D). Insikter Tryck på > Insikter i
  • Eco Mode

    Wiser Home – System User Guide (Spain and Portugal)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Limitations of the Wiser System

    Wiser Home – System User Guide (Sweden, Finland)

    Lights Maximum overall Maximum per Room Lighting devices 32 32 Shutters Maximum overall Maximum per Room Shutter Devices 32 32 Appliances Maximum overall Maximum per Room Any combination of the following ON/OFF appliances Connected Sockets Smart Plugs Wiser Power Micromodule 20 20 1-gang / 2-gang
  • Eco Mode

    Wiser Home – System User Guide (Denmark)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
Page 64 of 110