Showing 681 - 690 of 1,241 results

Page 69 of 125
  • Insights

    Wiser Home – System User Guide (Denmark)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Om enheden

    Wiser Smat Plug 16 A – Brugervejledning til Wiser Home-enheden

    Om enheden Om enheden Om enheden Wiser Smart Plug (herefter kaldet stik) bruges som stikadapter til at styre forskellige elektriske enheder som f.eks. gulvlamper, radioer eller kaffemaskiner manuelt eller ved hjælp af Wiser-appen. Stikket kan også overvåge strømforbruget for tilsluttede enheder
  • Wiser Plug Wiser Home Device User Guide

    smart plug to flammable liquids, gases or other explosives. Failure to follow these instructions can result in injury or equipmentdamage. DUG_Wiser Plug_WH-10 5 About the document https://www.se.com/ww/en/work/support/country-selector/select-your-location.jsp https://www.se.com/ww/en/work/support
  • Acerca del documento

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Acerca del documento Acerca del documento Acerca del documento Objeto Este documento proporciona orientación sobre la instalación, puesta en marcha y uso del cargador de vehículos eléctricos EVlink Home Smart con la app Wiser Home. Explica cómo configurar los ajustes de red, gestionar los modos de
  • Anti-Tripping Management

    Wiser Home – System User Guide (France)

    executed. Maximum of 8 devices can be added. Supported devices: Power Micromodule (Water Heater) EV Socket Smart Plug Connected Sockets Schneider Charge Pre-requisite: Configure one of your PowerTag as Grid. Refer to Pairing main PowerTag. Set the Contract limit. A default contract limit is
  • Anti-Tripping Management

    Wiser Home – System User Guide (Germany, Austria)

    executed. Maximum of 8 devices can be added. Supported devices: Power Micromodule (Water Heater) Smart Plug Connected Sockets Schneider Charge Pre-requisite: Configure one of your PowerTag as Grid. Refer to Pairing main PowerTag. Set the Contract limit. A default contract limit is automatically set
  • Creating an automation

    Exxact - Connected Double Socket Outlet 16A – Wiser Home Device user guide

    actions within an automation. In this example, we will initially select Control a device and select Smart Socket (F) as the device to trigger an action, later, we will select for the Wait option to add a delay in the automation. You cannot select the same device that you selected for Add conditions in
  • Energiöversikt

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    varje timme, så fluktuationer är normalt. Systemet använder en smart algoritm för att bara räkna tiden när Wisers smarta funktioner aktivt sparade energi. Tryck på frågetecknet (A) för mer information. Uppvärmningstider (B): Detta avsnitt visar hur mycket uppvärmningstid du har använt, i förhållande
  • Insikter

    Wiser Home – Systemanvändarhandbok (Sverige, Finland)

    Home Smart, Schneider Charge, EV-uttag) eller resistiva vattenpannor (som styrs med en strömställarpuck). Den förlitar sig på att användarna svarar på rutinfrågor. Se Wiser Home AI för detaljerad information. Du kan ändra den visade tidsramen (dagar, månader och år). Om du har installerat PowerTag på solenergi eller solenergi med batteri är Mina besparingar tillgängligt för att visa spar- och intjäningshistorik.
  • Aikataulun määrittäminen

    Exxact - kaksoispistorasia 16A – Wiser Home -laitteen käyttöopas

    -valikkoon. Valitse Smart-pistorasia kohteesta KOSKEE valikko ja napauta Luo. Seuraavassa näytössä näkyy oletuksena viikon tapahtuma, jota voi muokata. Napauta jos haluat lisätä tapahtuman, kuten TILA (päällä/pois) ja AJANKOHTA (auringonnousu/auringonlasku tai tietty aikaväli). Tallenna aikataulu
Page 69 of 125