Showing 691 - 700 of 1,241 results

Page 70 of 125
  • Informações

    Wiser Home – Guia do Utilizador do Sistema (Espanha e Portugal)

    registar os dispositivos de alta energia como Carregador VE (Evlink Home Smart, Schneider Charge, tomada VE) ou caldeiras de água resistiva (controladas por um Micromódulo Potência Wiser). Depende dos utilizadores para responder a perguntas de rotina. Consulte Wiser Home IA para obter informações
  • Google Home™

    Wiser Radiator Thermostat – Wiser Home Device user guide

    Google Home™ Google Home™ Google Home™ Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.” Common Wiser commands for Google Home™: Inquiry: “OK, Google, is the
  • About the device

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Modo de carga

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    Modo de carga Modo de carga Modo de carga Con la aplicación Wiser Home, puede administrar el modo de carga. En la pestaña Control, pulse Todos los dispositivos > EVlink Home Smart. En la página del panel de control del dispositivo, toque Modo de carga. En el menú EV Charging Mode, seleccione una
  • Insights

    Wiser Home – System User Guide (Denmark)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Wiser Home System User Guide (Spain and Portugal)

    System 3. Tap Devices. List of Devices: Back Settings Account Rooms Devices Away Mode Smart Modes System settings Support Home Screen App VersionX.Y.Z (Build XX) App Theme 78 SUG_Wiser_Home_Iberic_WH-08 Configuring the Wiser System A The battery charge level indicator which displays the current battery
  • Affichages LED

    Wiser détecteur de fumée connecté sur secteur 230V – Guide de l'utilisateur de l’appareil Wiser Home

    désactivation Niveau de piles faible Clignote toutes les 24 s ARRÊT 10 h Défaut 2 clignotements toutes les 24 s ARRÊT 10 h Mémoire d’alarme Clignote toutes les 48 s ARRÊT 10 h Pour tous les modes de fonctionnement, la LED clignote en rouge. * Pour les détecteurs de fumée locaux, toutes les LED rouges clignotent, tandis que pour les alarmes de température locales, seule la LED rouge En attente clignote.
  • Eine Automatisierung erstellen

    Wiser Smart Plug 16A – Wiser Home Geräte-Benutzerhandbuch

    Verzögerung in einer Automatisierungssequenz hinzufügen. Sie können die Wartezeit in Schritten von 1 Stunde und 1 Minute bis zu maximal 24 Stunden einstellen. Diese Funktion ist nützlich, um Aktionen innerhalb einer Automatisierung zu verzögern. Tippen Sie auf Steuerung eines Geräts > Smart Plug
  • Exemplo de uma automatização

    Tomada Wiser – Guia do utilizador do dispositivo Wiser Home

    > Modo Ausente > Modo Ausente ativado (A). Leia as informações e toque em OK. Para definir a hora, toque em Quando > Adicionar tempo > Período de tempo > Dia > Definir. Para adicionar uma ação, toque em Então > Adicionar uma ação > Controlar um dispositivo > Tomada smart >
  • About the device

    Unica - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
Page 70 of 125