Showing 761 - 770 of 1,241 results

Page 77 of 125
  • Configuring UFH actuator

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    temperature.The thermostat can also be used as a temperature sensor and a temperature set point selector for other heating devices like 16A Relay or ELKO - Smart Radiator Thermostat. Refer, pairing the device. Refer, . Assign a room to the thermostat once it has been paired and then tap Next to configure
  • Setting up a schedule

    Exxact - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Setting up a schedule Setting up a schedule Setting up a schedule Using the Wiser Home app, you can create or assign a schedule to the Socket outlet. On the Home screen, tap . Go to Schedule tab, tap . Enter the Schedule name and select Appliances from the TYPE menu. Select the Smart Socket Outlet
  • Troubleshooting

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    highly reflective surface. Ensure there are no swaying objects within the detection range. Check that the load is not wired directly to the power supply. Lighting turns on and off Quickly TIME set too short False trigger Wrong modes (Short pulse mode or Test mode) Ensure sensor is away from heat source
  • Automaation poistaminen

    EVlink Home Smart – Wiser Home -laitteen käyttöopas

  • Automatisering

    EVlink Home Smart – Brugervejledning til Wiser Home-enhed

  • Gepersonaliseerde energie-inzichten (Geschatte energie)

    PowerTag Energy – Wiser Home Gebruikershandleiding voor het apparaat

    een hoog verbruik voor de geselecteerde tijdsperiode. De belastingen die bovenaan verschijnen, zijn gebaseerd op het gebruik over het hele bereik. Als bijvoorbeeld Evlink Home Smart in oktober niet veel wordt gebruikt, wordt het getoond in de (D) kaart Andere. De geüpdatete verbruikswaarde wordt
  • About the device

    System M and System D- Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    Zigbee network. The device can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to install on the wall: no
  • Eco Mode

    Wiser Home – System User Guide (France)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
  • Personliga energiinsikter (uppskattad energi)

    PowerTag Energy – Wiser Home Bruksanvisning för enheten

    över hela området. Om EVlink Home Smart till exempel inte används mycket i oktober visas det i kortet Andra (D). Det uppdaterade förbrukningsvärdet visas i uppdelningsdelen när du rullar ned. De anpassade etiketterna för laster är grupperade i uppdelningen Andra (D). Insikter Tryck på > Insikter i
  • Eco Mode

    Wiser Home – System User Guide (Spain and Portugal)

    Eco Mode Eco Mode Eco Mode Eco Mode is a smart feature designed to maximize the efficiency of your heating system. It automatically optimizes the stop time of the heating phase, each time the set temperature changes from a higher to lower value. Eco Mode is a system feature that is either activated
Page 77 of 125