Showing 781 - 790 of 1,622 results

Page 79 of 163
  • LED indications

    Ovalis - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off. Resetting
  • Insights

    Wiser Home – System User Guide (UK, Ireland)

    saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings. C Tracks adjustments made to heating, including the number of times the heating was turned up or down, as well as
  • Insights

    Wiser Home – System User Guide (France)

    timeframe (days, months and years). B Shows the percentage of energy saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings. C Tracks adjustments made to heating, including the
  • Affichages LED

    Capteur de fuite d’eau Wiser – Guide de l'utilisateur de l’appareil Wiser Home

    Affichages LED Affichages LED Affichages LED Appairage Action de l'utilisateur Affichage de la LED Statut Appuyez 3 fois sur la touche de fonction La LED clignote en orange une fois par seconde. Le mode d'appairage est actif pendant 30 secondes. Une fois l’appairage terminé, la LED s’allume en vert
  • Insights

    Wiser Home – System User Guide (Sweden, Finland)

    timeframe (days, months and years). B Shows the percentage of energy saved for the current month, along with a 3-month average comparison. It also provides data on hours saved in Away Mode and allows you to enable Eco Mode for additional savings. C Tracks adjustments made to heating, including the
  • Gerät verwenden

    Schneider Wechselrichter und Boost – Wiser Home Geräte-Benutzerhandbuch

  • Device

    Wiser Home Essential API – User Guide

    Device Device Device The following topics are examples of fetching a list of devices, device details, and the away mode status.
  • Creating an automation

    LK FUGA® Wiser wireless PIR with relay – Wiser Home Device user guide

    . Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide. Tap Device status change > Motion Switch and select any of the following options: Switch On/Off: Select the device
  • Eine Automatisierung erstellen

    Wiser Heizkörperthermostat – Wiser Home Geräte-Benutzerhandbuch

    Gerät steuern > Heizung→und wählen Sie eine der folgenden Optionen (H): Boost: Stellen Sie die Dauer so ein, dass die Temperatur um 2 °C erhöht wird. Sollwert: Stellen Sie die gewünschte Temperatur ein. Tippen Sie auf Sollwert, stellen Sie die gewünschte Temperatur mit dem vertikalen
  • Google Home

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    , aber kein Temperatursollwert angegeben wird, setzt Google Home die neue Solltemperatur auf den vorherigen Sollwert ±3 Grad. Dieser Wert wird von Google Home gesteuert und unterscheidet sich von einem normalen Wiser-Boost, der den neuen Sollwert standardmäßig auf ±2 Grad über/unter der aktuellen
Page 79 of 163