Showing 811 - 820 of 1,449 results

Page 82 of 145
  • Exxact - Connected Blind Control Switch

    Schneider Electric Shutter Calibration without Wiser app Shutter Calibration without Wiser app Schneider Electric 35 rue Joseph Monier 92500 Rueil Malmaison France + 33 (0) 1 41 29 70 00 www.se.com Schneider Electric Seasonal Comfort Mode Seasonal Comfort Mode Schneider Electric 35 rue Joseph
  • Resetting the device manually

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    Resetting the device manually Resetting the device manually Resetting the device manually Short press (< 0,5 s) the Setup/Reset button 3 times and then long press the Setup/Reset button once for >10 s to reset the smoke alarm to factory default mode. All configuration data, user data and network data are deleted.
  • Création d’un programme

    EVlink Home Smart – Guide d'utilisation de l'appareil Wiser Home

    l'onglet Contrôle, appuyez sur Tous > EVlink Home Smart. Appuyez sur Mode en charge. Si EVlink Home Smart est installé avec Wiser Hub, vous pouvez également naviguer sur le chemin suivant pour créer des horaires : Sur l’écran d’ accueil, appuyez sur . Appuyez sur Programmes > Programme Véhicule
  • Création d’un programme

    Schneider Charge – Guide de l'utilisateur de l’appareil Wiser Home

    l'onglet Contrôle, appuyez sur Tout > Schneider Charge. Appuyez sur Mode de charge. Si Schneider Charge est installé avec Passerelle Wiser, vous pouvez également naviguer sur le chemin suivant pour créer des programmes : Sur l’écran d’ accueil, appuyez sur . Appuyez sur Programmes > Programme
  • Setting the room temperature using the app

    Wiser Radiator Thermostat – Wiser Home Device user guide

    the bar activates Frost Protection mode. In this mode, the system maintains the room temperature at a constant 5 °C to prevent freezing. You can also adjust the room temperature: By tapping or on the Control tab, in the Heating section of the concerned room to adjust its temperature. If you only
  • Troubleshooting

    Wiser Home – System User Guide (France)

    use devices listed in List of Wiser Devices. The device is not able to connect with the Hub /Hub R. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should
  • Troubleshooting

    Wiser Home – System User Guide (Germany, Austria)

    use devices listed in List of Wiser Devices. The device is not able to connect with the Hub. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should reboot into
  • Troubleshooting

    Wiser Home – System User Guide (Spain and Portugal)

    use devices listed in List of Wiser Devices. The device is not able to connect with the Hub /Hub R. After pressing 3 times, the device LED blinks amber for 30 s. Pairing mode has changed. Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should
  • Schedules

    Wiser Home – System User Guide (Sweden, Finland)

    schedule. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities . Schedules are created and edited on the Automation screen (A) Tap a Schedule to navigate to the Schedule details. Schedule details: A Device type A Schedule can
  • Schedules

    Wiser Home – System User Guide (Denmark)

    schedule. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities . Schedules are created and edited on the Automation screen (A) Tap a Schedule to navigate to the Schedule details. Schedule details: A Device type A Schedule can
Page 82 of 145