SUG_DA_WH-04

Schedules

Set a Schedule to define the specific time for changing the state of the device.
TIP: The Schedule changes the device's state based on the events set at a chosen time. If you need to reverse/change the state at a different time, add another schedule event.
  • Example 1:

    Event 1: Set heating to 19 °C at 6:30.
    Event 2: Set heating to 15 °C at 8:30.


    Result: This action maintains the temperature at 19 °C from 6:30 to 8:30, and at 8.30, it changes to 15 °C.

  • Example 2:

    Event 1: Set kitchen light to 'ON' at 19:00.
    Event 2: Set kitchen light to 'OFF' at 23:00.

    Result: This action keeps the kitchen light ON from 19:00 to 23:00, and at 23:00, the kitchen light turns OFF.

NOTE: The new action always overrides the current action. Therefore, if a new event is added to the device or manual operation occurs while a scheduled action is in progress, the system will stop the ongoing schedule. For a detailed understanding of which action/control mode takes precedence over others, refer to Understanding Control Mode Priorities .

Schedules are created and edited on the Automation screen (A)

Tap a Schedule to navigate to the Schedule details.

Schedule details:

A

Device type

A Schedule can only be set for one specific Device type.

B

Name of the Schedule

C

Devices the Schedule applies to

D

Event list

The events of the Schedule are listed here, sorted by day of the week.

The bars give an overview of the status of the device during an event (e.g. full green bar when shutter fully open).

The time of the event is shown next to the bar.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.