Showing 8,161 - 8,170 of 9,888 results

Page 817 of 989
  • Away Mode

    Wiser Home – System User Guide (Belgium)

    Away Mode Away Mode Away Mode The Away Mode is designed to set your home in a sensible state when you are away for longer periods (e.g. being away for the weekend). It temporarily overrides the normal controls (e.g. moments, automation) implemented in the hub. When you disable away mode, the
  • LED-valon kirkkauden säätö

    Wiser-palovaroitin 230 V – Wiser Home -laitteen käyttöopas

    . Muussa tapauksessa voit odottaa 30 s, että valmiustilan LED-valo sammuu, ja sitten kirkkaustaso tallennetaan. LED-valon kirkkauden muuttaminen sovelluksella Valitse aloitusnäytössä . Valitse Laitteet Palovaroitin LED-merkkivalo (A). Paina lyhyesti Asetus/nollaus (S/R) -painiketta laitteella herättääksesi sen ennen kirkkaustason muuttamista. Valitse sovelluksessa jokin seuraavista (B): Maksimi Vähintään Valitse OK.
  • Styra rörelsesensorn

    ARGUS rörelsesensor utomhus 360 – Bruksanvisning för Wiser Home-enhet

    att vara tillgängliga via startskärmen. Välj önskad rörelsesensor i listan (A). Välj den tid som den anslutna enheten ska vara aktiv. Om det behövs trycker du på enhetsikonen för att aktivera eller inaktivera den.
  • Pairing Wireless Switch with Push-button Dimmer

    Exxact - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    Dimmer 5 times in quick succession. The status LED blinks green. The light connected to the Push-button Dimmer blinks for a few times. The status LED stops blinking green on the Wireless switch and the Push-button Dimmer. The Push-button Dimmer can now be controlled by the Wireless switch.
  • Google Home

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enhet

  • Setting the motion detection timer

    Unica - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

  • Setting the threshold temperature

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    Setting the threshold temperature Setting the threshold temperature Setting the threshold temperature Using the Wiser Home app, you can define the inside and outside temperature of a room above which the shutters shall close. To set the threshold inside and outside temperature: In the Seasonal Comfort Mode set-up page, tap Temperature. Set the inside and outside desired temperatures and tap Set.
  • Jalousie mit Kipplamellen

    System M und System D - Connected Taster-Modul, 1fach/2fach – Wiser Home Geräte-Benutzerhandbuch

    Jalousie mit Kipplamellen Jalousie mit Kipplamellen Jalousie mit Kipplamellen Tippen Sie auf dem Startbildschirm auf . Tippen Sie auf Geräte Jalousien Jalousie mit Kipplamellen. Tippen Sie auf Dauer Öffnen/ Dauer Schließen (A) und geben Sie die aufgezeichnete Öffnungs-/Schließzeit der Jalousie ein
  • Indicações do LED no Quick Home Connect

    Sistema M e Sistema D - Botão de pressão conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    Indicações do LED no Quick Home Connect Indicações do LED no Quick Home Connect Indicações do LED no Quick Home Connect Emparelhar o dispositivo no Quick Home Connect Ação do utilizador Indicador LED Estado Prima 5 vezes o botão de pressão numa sequência rápida. O LED pisca a verde uma vez por segundo. O modo de emparelhamento fica ativo durante 60 segundos. Quando o emparelhamento estiver concluído, o LED para de piscar.
  • LED-Anzeigen

    Wiser Funkempfänger 16 A für Temperaturregelung – Benutzerhandbuch des Geräts

Page 817 of 989