Showing 891 - 900 of 1,622 results

Page 90 of 163
  • Using the device

    EVlink Home Smart – Wiser Home device user guide

    E, F, G, H, J. A Total cost of charging session. B Total time of charging in the session. C Total energy consumption in the session. D Control button (Start charging/Stop charging, Pause/Resume). E To select the charging mode. Refer to Charging mode. F To see the 24 hr schedule based on the
  • Using the device

    Mureva EVlink – Wiser Home Device User Guide

    options E, F, G, H, J. A Total cost of charging session. B Total time of charging in the session. C Total energy consumption in the session. D Control button (Start charging/Stop charging, Pause/Resume). E To select the charging mode. Refer to Charging mode. F To see the 24 hr schedule based on the
  • Configuring the device

    Exxact - Connected Multiwire Universal Push-button Dimmer LED – Wiser Home Device user guide

    of the device. B Location: Tap to assign the dimmer to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C RL-LED Mode: You can improve the dimming quality in the app if you have problems with light flickering. Tap the toggle switch to
  • LED Indications

    Exxact - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees. Away mode Status User Interaction Description Away mode is set in Wiser Home app. A dot-matrix display glows, indicates that the thermostat is in away mode.
  • Creating an automation

    Exxact - Connected Motion Sensor with Push-button Dimmer LED – Wiser Home Device user guide

    . Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide. Tap Device status change > Motion Dimmer and select any of the following options: Dimmer On / Off: Select the dimmer
  • Creating an automation

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    . Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide. Tap Device status change > Motion Dimmer and select any of the following options: Dimmer On / Off: Select the dimmer
  • Creating a moment

    Wiser Room Thermostat – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • Creating a moment

    Wiser Flush-mounted Thermostat 2 A – Wiser Home Device user guide

    device to set the condition. For example, select heating. Set the required temperature using sliding control (D). When you put the slider control (D) at the bottom of the bar for the moment, the Frost Protection mode is activated. In the frost protection mode, the system maintains the room temperature at
  • LED Indications in Quick Home Connect

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
  • LED Indications in Quick Home Connect

    Odace - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    LED Indications in Quick Home Connect LED Indications in Quick Home Connect LED Indications in Quick Home Connect Pairing the device in Quick Home Connect User Action LED Indication Status Press the push button 5 times in quick succession. LED blinks green, once per second. Pairing mode is active for 60 seconds. When pairing is completed, LED stops blinking.
Page 90 of 163