DUG_EVlink_WH-07

Using the device

The Control Panel allows you to start and stop charging and monitor the power consumption.

On the Control page, tap EVlink Home Smart to access the control panel.

On the control panel page,

  • You can see the options A, B, C, D.

  • Tap to see the options E, F, G, H, J.

A

Total cost of charging session.

B

Total time of charging in the session.

C

Total energy consumption in the session.

D

Control button (Start charging/Stop charging, Pause/Resume).

E

To select the charging mode. Refer to Charging mode.

F

To see the 24 hr schedule based on the electricity rates.

G

To see the history. Refer to History.

H

To add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide.

J

You can rename the device or remove the device from the Wiser system. Refer to Renaming the device and Removing the device .

Similarly, you can control and check the current status from Control page.

  • Control button (H).

  • Current state of the device (I).

TIP: You can also start and stop charging when you add the device to your Favorite list.
NOTE:
  • If you only have an EVlink Home Smart in the Wiser System, the Control page will not be visible. All functions will be accessible through the Home page.

  • Electric vehicles (EV) can't be charged immediately after they have stopped. Reconnect the plug to start charging. Refer Connecting/disconnecting the charger.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?