Showing 91 - 100 of 328 results

Page 10 of 33
  • Mode Absence

    Wiser Home – Guide de l’utilisateur du système (France)

  • Device

    Wiser Home Essential API – User Guide

    Device Device Device The following topics are examples of fetching a list of devices, device details, and the away mode status.
  • Creating an automation

    ARGUS Motion Sensor Outdoor 360 – Wiser Home Device user guide

    status change: To select a device to enable automation. Away Mode: To turn OFF the motion sensor and the device connected to it by enabling the this mode is enabled. When the away mode is triggered, sensitivity of the motion sensor turns OFF. You can enable the motion sensor and the device connected
  • App Settings

    Wiser Home – System User Guide (France)

    Micromodule). Refer to Wiser Home AI for detailed information on Reduce my Bill. Rooms List of all Rooms of your Home. Access to Room options. Devices List of all Devices of your Home. Access to Device options. Away Mode Specify what happens when you activate the Away Mode, like temperature setting
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Germany, Austria)

    away mode, changing the settings manually, or activating specific moments. However, if the Anti-Tripping Management is activated due to high power usage, it will override the manual override to prevent overloading of electrical system. Scenario 1: The charger is scheduled to start at 10 PM. At 6 PM
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Spain and Portugal)

    away mode, changing the settings manually, or activating specific moments. However, if the Anti-Tripping Management is activated due to high power usage, it will override the manual override to prevent overloading of electrical system. Scenario 1: The charger is scheduled to start at 10 PM. At 6 PM
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Sweden, Finland)

    , overriding any pre-existing schedules or automated controls in place at the same time. It is considered an override if the device has a predefined schedule that is active. This is typically the most recent action triggered on the device, such as setting the device to away mode, changing the settings manually
  • Understanding Control Mode Priorities

    Wiser Home – System User Guide (Denmark)

    , overriding any pre-existing schedules or automated controls in place at the same time. It is considered an override if the device has a predefined schedule that is active. This is typically the most recent action triggered on the device, such as setting the device to away mode, changing the settings manually
  • Creating an automation

    Airzone Plenum and Aidoo Pro - Air conditioner – Wiser Home Device user guide

    of the following (D): Device status change (Select the device) Away Mode (Enable or Disable) Maximum 10 conditions can be added. Select a device (E) that will set the condition. If you have selected the condition as Away Mode and action as Control a Device then this automation will override your Away
  • LED Indications

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    temperature limits -9 °C to 99 °C. The thermostat matrix display flashes “+ +” when the temperature is above 99 degrees. Away mode Status User Interaction Description Away mode is set in Wiser Home app. A dot-matrix display glows, indicates that the thermostat is in away mode.
Page 10 of 33