Creating an automation
- On the Home screen, tap
.
- Select Automation >
to create an automation.
- Enter the automation name (A).
- Tap If (B) and select any of the
conditions (C):
-
All conditions: To trigger an action when all the defined conditions are met.
-
Any condition: To trigger an action when any of the defined condition is met.
-
- Tap Add conditions and select any
of the following (D):
-
Device status change: To select a device to enable automation.
-
Away Mode: To turn OFF the motion sensor and the device connected to it by enabling this mode. When the away mode is triggered, sensitivity of the motion sensor turns OFF.
TIP: You can enable the motion sensor and the device connected to it by increasing the sensitivity level of the motion sensor. Refer to Setting the sensitivity for more details on how to set sensitivity.
NOTE: Maximum 10 conditions can be added.TIP: Away mode can also be used as a trigger to turn OFF the lights, dimmer or closing the gate etc. For more information refer to the Away Mode. -
- If you select Device status change tap Outdoor Motion Sensor.
- You can choose and update the following configurations
of the motion sensor that will trigger the automation:
- Motion detection
- Lux level
- Temperature threshold.
NOTE: There is a default setting for each of the configurations.
- Tap Set.
- To set a specific time to trigger the automation, tap and select any of the following (E):
- Tap Set.
- To add an action, tap Then > Add an action and select any of the following (F):NOTE: Maximum 10 actions can be added.
-
Control a device - Select the device which should be activated when the automation is triggered and set the desired state of the device.
-
Send notification - You will be notified if the automation is triggered.
-
Activate a moment - Select a moment to activate during the automation.
-
Wait - This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
Below is the example to trigger an action for the shutters using Control a device option:- On the New automation page, select Control a device and choose Shutter.
- Set the desired state of the shutter when the automation
is triggered. Then, tap Set.
Below is the example to use the Wait option:- On the New automation page, tap Add an action and select Wait.
- Scroll through the minutes and seconds to set the desired wait time. Then, tap Set.
-
- Tap the icon (G) to display the icon which best represents the automation.
- Select the icon from the Choose an icon page and tap Save to set the icon.
- On the New automation page, tap Save.Once the automation is saved, it is visible in the list of automations.
- Tap the toggle switch (H) on the Automation page to enable/disable the automation.