DUG_Connected Thermostat 16 A, ZB_WH-05

Amazon Alexa™

Amazon Alexa™ (Alexa) is an intelligent personal assistant developed by Amazon™, and is capable of voice interaction.

Common Wiser commands for Alexa

  • Discover Devices: “Alexa, discover devices”

  • Reduce Temperature: “Alexa, decrease the temperature upstairs by 4 degrees”

  • Increase Temperature: “Alexa, increase the temperature upstairs by 3 degrees”

  • Set Temperature: “Alexa, set the upstairs to 20 degrees”

  • Get Temperature: “Alexa, what is the upstairs temperature?

  • Get the Set Point: “Alexa, what is the upstairs set to?”


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?