DUG_Unica PB Dimmer_WH-08

Troubleshooting

Symptom

Solution

Dimming up not possible.

  • Reduce/increase load.

  • Allow the Dimmer to cool in case of overheating.

  • Change the load (if the load is incompatible with the Dimmer).

Switching On not possible.

  • Allow the Dimmer to cool in case of overheating.

  • Reduce load.

  • Change load.

  • Check wiring between the push button and the Dimmer.

Flickering at minimum brightness.

  • Increase minimum brightness (if flickering still persists, install a 31LCDA load correction device).

  • Change the load (if the minimum brightness is insufficient).

  • Set to RL LED mode.

Flickering

Only slight dimming capability

  • Change dimming range.

  • Set to RL LED mode.

  • Change the load (if the load is incompatible with the Dimmer).

The device is not ready to pair after the device is removed from the app.

Reset to factory default settings, refer to reset the device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.