DUG_Connected Thermostat 16 A, ZB_WH-03

Creating a Schedule/Event

The device can be fully controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.

To create the schedule/event:

  1. On the Home page, tap .

  2. Tap on the Schedules tab > .

  3. On the New Schedule page, enter the Schedule name, select Type, and select room.

  4. Tap Create.

  5. Select any day (A) and tap for add event:

    • Select temperature (for example 16 °C).

    • Set time (for example 12:00).

      NOTE: A maximum of 8 events can be created per day.

      You can tap to copy the schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one.

  6. Tap Set.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?