DUG_Micro Module Dimmer_WH-03

Resetting the device manually

Select any one of the options to reset the device to factory default mode:

  • Short press the Setup/Reset button 3 times and then long press the Setup/Reset button once for 10 s on the puck with a screwdriver.

  • Short press the push button 3 times and then long press the push button once for 10 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?