DUG_Micro Module Dimmer_WH-07

Adjusting the brightness level using app

By using the Wiser Home app, increase/decrease the brightness level in the Puck.
  1. Go to the Control tab, tap All devices or the room tab where the Puck is located.
  2. On the Device Control Screen, drag the sliding bar up/down to increase/decrease the brightness (A).
    TIP: You can also turn on/off the Puck on the Device Control Screen, tap (B) to turn on/off.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?