DUG_Micro Module Dimmer_WH-07

Setting the minimum and maximum brightness level

If the dimmer is connected to an LED, the minimum and maximum brightness should be set to avoid flickering and switching off the LED.
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule Dimmer .
  3. Drag the slider bar to increase or decrease the Minimum Brightness and Maximum Brightness (A).
    IMPORTANT: If the light does not begin to brighten up from 0%, adjust the minimum level setpoint to the point where the light actually starts to brighten. Similarly, for maximum brightness, set the maximum level based on the behaviour of the connected light. For example, if brightness does not increase between 80% and 100%, then set the maximum level to 80%.
    NOTE: The minimum brightness must be lower than the maximum brightness.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?