DUG_Micro Module Dimmer_WH-07

Setting up a schedule

The devices can be fully controlled by schedule. Once the schedule is set, the devices operates at a given time.
To create a schedule:
  1. On the Home screen, tap .
  2. Go to Schedules > to create a schedule.
  3. Enter the name of the schedule (A).
  4. In the TYPE menu, select Lights (B).
  5. In the APPLIES TO menu, select Micromodule Dimmer (C) from the listed devices.
  6. Tap Create to setup events.
  7. Tap to add an event such as STATE (lights off or dimming level in %) and WHEN (sunrise/sunset or specific time range).
    NOTE: Tap to copy the schedule from one day to other days or copy the entire schedule to a new schedule or to an existing one.
  8. Tap Set to save the schedule.
    TIP:
    • You can add multiple schedules based on your requirement. Select days, tap , set ON/OFF state and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?