DUG_Connected Thermostat 16 A, ZB_WH-03

Setting the device location

You can change the device location using Wiser Home app (such as bedroom, living room, dining room etc.).
  1. On the Home page, tap .
  2. Tap Devices, select the device from the list for which you wish to change the location.
  3. Tap Location to open setup page.
  4. On setup page, you can enter New room name (A) or select an existing room from the list (B).
    TIP: If the device is already assigned, you can remove it from the existing room. Tap Remove from Room (C).
  5. Once changes are done, tap Submit (D).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?