Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser Home app, you can create automations based on your needs.
  1. On the Home screen, tap .
  2. Go to Automation > to create an automation.
    NOTE: Maximum 10 automations can be added.
  3. Tap If (A) and select any of the following conditions (B):
    • All conditions: This triggers an action only when all conditions are met.
    • Any condition: This triggers an action when at least one condition is met.
  4. Tap Add conditions and select any of the following (C):
    • Device status change: Select a device to enable automation.
    • Away Mode: Enable/Disable away mode to trigger an action.
      TIP: Away mode can also be used as a trigger to turn off the lights, dimmer or closing the shutter etc. For more information about Away Mode, refer to the system user guide.
  5. Tap Device status change > Temperature/Humidity Sensor > TemperatureClimate, Set the temperature using sliding bar (D) and select the condition (E) (less than / more than), then tap Set.
    NOTE:
    • Maximum 10 conditions can be added

      .
    • To remove an added condition, swipe left and tap .

  6. To set a specific time for your automation, tap When > Add time and select any of the following (F):
    • Specific time of the day: Sunrise, Sunset, Custom.
    • Period of time: Daytime, Night time, Custom.
    NOTE:
    • Maximum 10 entries can be added

    • To remove a specific time, swipe left and tap .

  7. To add an action, tap Then > Add an action and select any of the following (G):
    • Control a device: Select a devices that you want to trigger.
    • Send notification: Turn on the notification for the automation.
    • Activate a moment: Select the moment that you want to trigger.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.

  8. Tap Control a device > Heating and select any of the following (H):
    • Boost: Set the duration to increase the temperature by 2° C.
    • Setpoint: Set the desired temperature.
  9. Tap Setpoint, set the required temperature using vertical sliding bar (I), then tap Set.
    NOTE:
    • Maximum 10 actions can be added.

    • To remove an action, swipe it left on the action and then tap .

  10. Enter the automation name (J).

    You can choose the cover image that represents your automation by tapping .

  11. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    Using the (K) you can enable and disable the automation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?