System User Guide Wiser Home (Germany, Austria) - 15

Setting up the Hub
/Controller

In order to be able to control the system via your smartphone, the hub
/controller
must be connected to the internet.

You can set up the Hub

/Controller
by using the app as Home Owner and Professional Installer.

The app offers the Professional Installer menu for setting up a Wiser System and adding devices without having to be logged in.

You can also setup the Wiser System by using the app as a Home Owner after creating an account. Refer to Setting up an Account for information on how to create an account.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.