System User Guide Wiser Home (Germany, Austria) - 15

Setting up as a Professional Installer

The app offers the Professional Installer menu for setting up a Wiser System and adding devices without having to be logged in.
NOTE: The option to act as a Professional Installer is only available if you are logged out of the app. To log out of the app, navigate to the Account settings and tap Logout.

To set up the Wiser System as Professional Installer:

  1. On the welcome screen, tap Get started (A).

  2. Tap Professional Installer (B).

  3. Select your country from the list.

The Add Devices screen allows you to add a hub

/controller
to the system. Refer to Connecting to the Hub's Temporary Wi-Fi® Network and Connecting to Wi-Fi® to add and setup the hub
/controller
.

For Hub 2nd Generation Only: You can also download firmware into your app that will update the hub during setup. See Downloading hub firmware into the app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.