DUG_Wiser Radiator Thermostat 2nd Generation_WH-00

About the device

The Wiser Radiator Thermostat 2nd Generation (hereinafter referred to as Thermostat) uses integrated temperature sensors to control the flow of water through a radiator, thereby regulating the temperature in a room. The target temperature and switching times are set by using the Wiser app.

Adding thermostats to your Wiser systems allows you to control schedules and temperatures in each room enabling personalized heating. This can help reduce energy usage significantly. The Thermostat provides individual room control with ultimate comfort, convenience, and practicality.

Thermostat features:

  • Twist-top radiator thermostat cap

  • Device user interface lock

Thermostat features in app:

  • Mobile control anytime, anywhere with the Wiser app

  • Works with Amazon Alexa and Google Assistant

  • Full transparency with Insights and the Heat Report

  • Smart modes for maximum energy efficiency

Operating elements

  1. Status LEDs

  2. Radiator Thermostat cap

  3. Ring nut (only used with M30 x 1.5 mm valve adapter)


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.