DUG_Wiser Radiator Thermostat 2nd Generation_WH-00

Setting the room temperature using the app

Using the Wiser Home app, you can adjust, set or boost the room temperature.

  1. On the Control tab, tap All Devices or select the room where the thermostat is installed.

    1. Use the slider to adjust the temperature.

      NOTE: A indicates that the room temperature is below the setpoint, and heating is currently ON.

      You can tap the boost icon to set a time duration for which the setpoint temperature will increase by 2 °C.

      IMPORTANT:
      • Moving the slider to the bottom activates Frost Protection mode, which maintains the room temperature at 5 °C to prevent freezing.

      TIP: You can also adjust the temperature on the control tab by tapping + or – in the Heating section of the selected room.
      NOTE: If your Wiser System has only one device, the Control tab will not appear. All functions will be available on the Home screen.
    2. Tap to set the time period to increase the setpoint temperature.

      IMPORTANT: Once this time is set, the setpoint temperature increases by 2 °C for the set boost time. After the boost, the setpoint temperature returns to the scheduled event or to the previous setpoint temperature.
      NOTE: You can stop the boost at any time by tapping and turning it off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.