DUG_Wiser Radiator Thermostat 2nd Generation_WH-00

Setting the room temperature manually

The room temperature can be increased/decreased manually by twisting the radiator thermostat cap.

Twist the radiator thermostat cap:

  • In the + direction: Increases the temperature. The red LED glows for 5 seconds.

  • In the - direction: Decreases the temperature. The blue LED glows for 5 seconds.

Every twist changes the setpoint temperature by ±2 °C from the current room temperature. This boost remains active for 1 hour.

NOTE: If the setpoint temperature is already more than 2 °C above or below the room temperature, the change will not adjust the setpoint temperature.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.