DUG_Wiser Smart Plug_WH-00

Identifying the device

Using the Wiser Home app, you can identify the Plug from the other available devices in the room.
To identify the Plug:
  1. On the Home screen, tap .
  2. Tap Devices > Smart Plug > Identify (A).
    NOTE:
    • This feature flashes the Plug green LED, so you can find the actual device. It may take up to a minute to start and flash the Plug LED.

    • The Plug LED will continue to flash until you tap OK

      .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.