For your safety

DANGER
Hazard of electric shock, explosion, or arc flash
  • It is illegal for persons other than an appropriately licensed electrical contractors or other persons authorised by legislation to work on the fixed wiring of any electrical installation.
  • To comply with all safety standards, the device must be used only for the purpose described in this instruction and must be installed in accordance with the wiring rules and regulation in the location where it is installed.
  • Lock out and tag the input circuit before accessing the wiring connections.
  • There are no user serviceable parts inside the device
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock
  • Make sure that the terminal connection area does not come in contact with the metallic parts of any device installed in the same location.
  • Do not short the outputs to neutral.
  • The switch contact and live conductor connection must be separated from one another by a 240 VAC basic insulation.
  • When working on the device, always disconnect the device from the power supply, as the output may carry electrical current even when the load is switched off
  • Isolate the incoming circuit before installation, maintenance, or service (or replacement of the load) of the device.
Failure to follow these instructions will result in death or serious injury.
CAUTION
THE DEVICE MAY BE DAMAGED
Please ensure that the device is disconnected from its circuit during the insulation resistance test.
Failure to follow these instructions can result in injury or equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?