Testing the device

Before using the module, manually test the module and make sure that it works when connected to the devices.

Short press the push button once, the connected device turns on/off.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?