Resetting the device

You can reset the device to factory default manually.
  1. Short press the push button 3 times and then long press the push button once for 10 s.
  2. After 10 s, LED starts blinking red then release the operation button.
    NOTE: All configuration data, user data, and network data are deleted.
    The LED stops blinking upon successful reset of the device.
    The module restarts and blinks green for a few seconds.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?